Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Undefined response from BlueNRG

Posted on November 28, 2017 at 06:56 Hello! I have a problem with BlueNRG chip (old one, NOT BlueNRG-MS). I made a custom PCB with STM32F407VGT6 and BlueNRG on it and try to setup. In MCU test firmware there aren't any functions that used for c...

BlueNRG-MS paring cancel issue

Posted on November 28, 2017 at 11:47Hi I have a BlueNRG-MS peripheral device, that requires pairing for encrypted data transfer.  Overall it works, but when cancelling the paring procedure from the central (IOS) then the following reconnect  attempt...

aes2 by Associate II
  • 1654 Views
  • 4 replies
  • 0 kudos

SPFW04 File creation

Posted on November 30, 2017 at 09:37Hello everybody!Is there a possibility in SPFW04 to POST and GET via HTTP not only from RAM, but from external SD card? Another question is whe i can`t create file bigger than 15360 bytes on external SD card?