Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Home Automation Profile H.A 1.2 with Zigbee Pro

I need to build a device with the Home Automation Profile (HA 1.2) . I would need help in order to select the proper Wireless MCU that could have the corresponding libraries and Zigbee Stack. Selection of the proper MCULibraries for that MCU with the...

Zartagal by Associate II
  • 1284 Views
  • 1 replies
  • 0 kudos

S2-LP strobe COMMAND_RX after DATA discarded EINT

Can someone tell me why the need to put the Receiver back in Receiver mode after getting a DATA_DISCARDED Interrupt, (many examples are using this), I'd like to only get interrupted when the preamble and sync bits match, I find it excessive (every fe...

xarion by Associate II
  • 1142 Views
  • 1 replies
  • 0 kudos

RSSI value of a node without mesh network

hello,I want to know if it is possible to get the RSSI value of a node with this function in BLUENRG-1 without the mesh network.tBleStatus hci_read_rssi (uint16_t Connection_Handle, uint8_t *RSSI);Can I use this if yes how? Because I am getting only ...

FChou by Associate II
  • 1459 Views
  • 2 replies
  • 0 kudos

SPWF01SA Deauthentication FW 3.6

Hi,I have a problem with SPWF01SA WiFi module with FW 3.6. The module is connected to a WiFi network, generated by a router (STAtion Mode), with active DHCP. A socket server is opened on port 80. I have seen that after a day the module IP is changed ...

Is it possible to perform asset tracking/indoor localization or to measure RSSI value on a BlueNRG-1/2 board in a bluetooth mesh network ?

I want to track/locate the position of a bluetooth mesh node. I am currently using three BlueNRG-1 based STEVALIDB007v1 boards and an android smartphone to form a bluetooth mesh network in which smartphone reads sensor data from mesh nodes. I did som...

MH1 by Associate II
  • 3135 Views
  • 8 replies
  • 0 kudos