Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPWF01SA Wind:5: Hardware Failure: 5

Hi everyone,Sometime when I try to connect the module to a exsisting WiFi network I receive the following string from the module:+WIND:0:Console active+WIND:32:WiFi Hardware Started+WIND:21:WiFi Scanning+WIND:35:WiFi Scan Complete (0xFF)+WIND:5:WiFi ...

Resolved! SPBTLE-1S - How to get a BLE connection?

Posted on January 07, 2018 at 03:06Hi, I just got the EVAL-IDB007V1M with the spbtle-1s (based on bluenrg-1 and installed the STSW-BLUENRG1-DK (v2.5.0) on my Windows PC. The BlueNRG-1 Navigator recognizes the EVAL-IDB007V1M and I can 'Flash & Run' t...

0690X00000609NSQAY.png 0690X00000609NXQAY.png

SPI interface between STM32F103C8 and ADE7758

Hi everyone,I have got some problems with programming SPI between ADE7758 (slave) and STM32F103C8 (master). I use build - in SPI (hardware SPI), and directly connect 4 pin (MOSI, MISO, NSS, CLK) to ADE7758 which is a 5V device without any conversion ...

mt.hust by Associate II
  • 3769 Views
  • 9 replies
  • 0 kudos

debug SSD1322 oled in 8080 mode

Hi I am using parallel bus to communicate with the OLED SSD1322 to display something, which include: DATA LINE0 to LINE7CSRDWRDM data or commandhowever , I could send the simple commands like display on , off to control the OLED after initializatio...

awu.2 by Associate II
  • 2182 Views
  • 3 replies
  • 0 kudos