Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TX_FIFO_ALMOST_EMPTY Interrupt Problem

hello,i work with the IDS014A4 SPIRIT1 WMbus board,i like to send a frame with the C1 mode(unidirectionel Sent)​.my first question is : why the Tx frame preparation is limited with12 bytes ?my programme can not sendall the data only when i replace :S...

OAhme by Associate
  • 659 Views
  • 0 replies
  • 0 kudos

Purpose of Smart Card Interface IC.

Hi AllIm relatively new to smart cards. Im wondering what is the purpose of using a Smart card interface IC such as the st8024 other than voltage adjustments? Would it not be easier to interface direct if the the intended smart card is a class B? 3V?

MWolm by Associate
  • 720 Views
  • 0 replies
  • 0 kudos

SPIRIT1 Example Code

I am adding the SPIRIT1 to legacy products that already have a specified MCU.  I have the purchased the full STEVAL-IKR002V3 Eval Kit and two additional daughter boards.  My MCU is able to read/write to the SPIRIT1 registers, but I cannot figure out ...

CKels by Associate
  • 2085 Views
  • 3 replies
  • 0 kudos

Resolved! STUSB1600 (USB Type-C) and USB OTG

I'm trying to understand how I can use a USB Type-C connector together with the STM32MP1 USB OTG peripheral.So obviously I want to use the port in dual role configuration. I want to use the STUSB1600 for that because it takes care of the power source...

arturo182 by Associate II
  • 11976 Views
  • 8 replies
  • 0 kudos

SPBTLE-1S, GPIOs

Hello,I am looking to prototype a project. I will need I2C, SPI and UART.  I2C for some ST sensors/gas gauge, SPI for sd card and UART for RS485.  Is it possible to use SPBTLE-1S, to run both host applications and bluetooth.  Thanks for your help

Sam Ho by Associate II
  • 1993 Views
  • 2 replies
  • 0 kudos