Blue NRG Tile sold individually?
I was wondering if the BlueNRG Tile is sold individually without the dev board?
Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.
I was wondering if the BlueNRG Tile is sold individually without the dev board?
HelloI measured the output power with several S2-LP development kits with the S2-LP DK – Application v1.2.1. If I set the HPM maximum output power of +14dBm, I can measure the following output power:KIT1 (STEVAL-FKI433V2): 12.9dBmKIT2 (STEVAL-FKI433V...
Hello Geeks!I have costume hardware for the STM32F429Zi.I'm using default HAL driver for the LWIP, generated from cubeMX (Nice tool) with FreeRTOS For the Ethernet link, my board has external phy ic that is LAN8742AMy aim is to detect the Ethernet ca...
Greetings,I am looking for a way to program into the Eval board IS31FL3741 so that I can control FxLED. I have tried controlling it externally using Arduino, but looking out for a way to dump the code into the Eval Board mentioned above. I tried con...
Hi Guys, There is so little information and examples available on this device I hope this forum can help.In all examples I have seen the code has and EXTI for when the S2LP reports a data discarded, thereafter you need to re-issue the command to Star...
I'm curious to know what data it sending while clicking on the particular button on BLE mesh app.I mean packet format while sending and receiving (for eg. It have destination address like that)
Hi,I'm using EVK (STEVAL-FKI868V2), loading the Binaries file to EVK All the command line function is ok. but when I use your sample code:File Location: C:\Program Files (x86)\STMicroelectronics\S2-LP_SigFox_DK_1.6.0\Projects\Projects_Cube\S2-LP_SigF...
I am using nucleo-l053r8 and i flash it with S2LP_CLI_NUCLEO_L0 firmware. But when trying to open the port: i always get the message "wrong firmware detected. Please click OK to start upgrade procedure..."I click OK, the firmware is succesfully flash...
I'm not able the see the x-cube-blemesh1 flashed code networks in other apps and phone bluetooth setting also . I'm trying to send the particular value from app to node and want to see that is received properly or not in node by debugging??How we can...
I am using STSW-BNRG-Mesh v1.07 embedded SDK.In vendor model client node, I use BluenrgMesh_SetRemoteData() function to set other vendor model server node. It works well if the target is not low power node. However, if the target is low power node, a...