cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-FKI868V1has feature'Automatic acknowledgement, retransmission, and timeout protocol engine'. Does this feature automatic for S2-LP transceiver or it may be enabled/disabled programmatically?

bvn123
Associate II

S2-LP transceiver, STEVAL-FKI868V1:

it has a feature 'Automatic acknowledgement, retransmission, and timeout protocol engine".

1. Does the acknowledgement automatically come from receiver?

2. Does this feature automatic for S2-LP transceiver or it may be enabled/disabled programmatically?

3. If I want to use a few receivers, is it possible to disable this feature or enable it only for one receiver, which is placed on the longest distance?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Winfred LU
ST Employee

Hi N.Vadim,

  1. Yes, if automatic acknowledgement is enabled
  2. Yes, please enable with register PROTOCOL0, bit 2
  3. Yes. please refer to the DK S2LPLibrary_Examples, STack LLP example

in SDK_StackLlp_B.c it enables the auto ack by default (line 379): S2LPPktStackAutoAck(S_ENABLE);

Please modify according your needs.

Best Regards,

Winfred

View solution in original post

3 REPLIES 3
xarion
Associate II

It depends on your mode, if you are using STack it does an automatic acknowledgement. If you don't want an ACK then use a basic configuration similar to the GUI.

Winfred LU
ST Employee

Hi N.Vadim,

  1. Yes, if automatic acknowledgement is enabled
  2. Yes, please enable with register PROTOCOL0, bit 2
  3. Yes. please refer to the DK S2LPLibrary_Examples, STack LLP example

in SDK_StackLlp_B.c it enables the auto ack by default (line 379): S2LPPktStackAutoAck(S_ENABLE);

Please modify according your needs.

Best Regards,

Winfred

bvn123
Associate II

Hi Winfred,

thank You very much,

it's rare to see such answers - all according to the questions and nothing redundant.

And it was very usefull for me to get the names of libraries and examples and ever line number in c-file !

Best regards,

Vadim