Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BLE_SensorDemo sensor updates to ST BLE Sensor app: I would like to increase the update frequency of BCN002V1 tile sensors (in particular the proxiity sensor) to the app. I'm looking for the timing code that controls the updates to the Android/iPhone app.

I can't get the data transmitted faster than every 487ms or about 0.5s. And that's with the Motion Sensor Update Rate set to 40Hz. I've set the DM (Distance Mode) to short (=1), the TimingBudget to 20 ms and the InterMeasurement down to 25ms. The rel...

RGupp by Associate II
  • 691 Views
  • 0 replies
  • 0 kudos

STSW-BLUENRG1-DK v3.0.0 doesn't run on windows 10

Hi,After downloading STSW-BLUENRG1-DK v3.0.0 and installing on my windows 10 PC I can't open BlueNRG-1_Navigator.exe. When I double click on it nothing happens. But BLUENRG1_Wizard.exe does work.During installation it failed to install the STMicroele...

CHossack by Associate III
  • 4325 Views
  • 14 replies
  • 2 kudos