User Activity

Hi! Is anybody have a schematic with a BALF-SPI2-02D3 + SAW FILTER? Is this wiring will be good?
Hi, is anyone try to use TCXO to S2LP? I designing a board with it. What should be the values of registers? It's for the 433MHz band.
Hi, I try to transmit data by S2LP(RC-S2LP-433) and have a problem. When I try to debug the unit (true studio) everything work great, when the TX end then get an ISR to reset flag and in main loop start new transmitt. When I try to start the unit wit...
Hello, can you help me recognize the S2LP version. I read the register DEVICE_INFO1 and I get 0x91 on the RC-S2LP-433 and in the Steval-fki433v2 is 0xC1. I have some problems with RC-S2LP and I think there is a different version of ic. Thx.