Skip to main content
WFerr.1
Visitor II
March 20, 2020
Question

Sensor Tile firmware stop working after a couple of debug connections - SysTick_Handler is never triggered.

After a couple of times that I reflashed the unit to debug, it became unresponsive. The first few times I got to download and debug the Sensor Demo project, the it stopped working alltogether. I got to connect the debugger and go step by step. In the file vl53l1_platform.c of the BLE_SensorDemo project, line 141, I noticed that the SystemClockTick is always 0 now. The interruption that causes the system tick to increment, SysTick_Handler, is never triggered. Obviously this is what prevents the firmware to work properly. What could cause this problem, especially considering that initially it was working as expected?

This topic has been closed for replies.