Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is L7987 Synchronous or Asynchronous?

Hi all,I am designing a 48 volt to 12 volt 3 amp DCDC asynchronous buck converter (with frequency > 200kHz) and I found the L7987. Although it says asynchronous in the datasheet, it looks like synchronous in the block diagram. I am confused, can some...

AziD32 by Associate
  • 2161 Views
  • 3 replies
  • 0 kudos

Need technical guidance for SCLT3-8BT8

I need to interface Digital input sensors of PNP & NPN type both in one of my product.Can I use SCLT3-8BT8 to interface both the type of sensors? Ho should we detect high side & low side through SPI lines on microcontroller?Thanks for your help in ad...

NDesh.2 by Associate II
  • 737 Views
  • 1 replies
  • 1 kudos

Sub1GHz module

Hi, I would like to explore the possibility of using the sub1GHz product solution from ST, particularly, the part number S2-LPTX.Here are the requirements1. We need One Receiver and 4 Transmitter (as shown in the image) which are operating at 433MHz ...

AshnoJames_0-1748435550932.png

STPM34 calibration formulas troubles

Hello! I try calibrate STPM34 device, but have some troubles.I created some xmls file with Reference Manual and AN4470 and compare results by STPM3x_Evaluation_Software and it different. 1) RM use default Vref value as 1.18, but App use 1.22) Calcula...

jspacy87 by Associate
  • 562 Views
  • 0 replies
  • 0 kudos

Resolved! STUSB1600

Hello,I have questions about the STUSB1600:1. Mouser marks the device as "obsolete". What is the EOL of the STUSB1600 and what alternative is recommended (STUSB1700?)?2. The STUSB1600 is connected to the MP1 via I2C. I need to program the NVM "in sys...

EOF by Associate III
  • 3732 Views
  • 10 replies
  • 1 kudos

BlueNRG-M2SA: DIO0 & DIO1 output problem

Hi,I'm trying to configure DIO1 and DIO0 as outputs in my custom board, but I can't get them to work. I'm using this basic code to test:SysCtrl_PeripheralClockCmd(CLOCK_PERIPH_GPIO, ENABLE); GPIO_InitOutputPinx(GPIO_Pin_6); GPIO_SetBits(GPIO_Pin_6); ...

reinoso by Associate
  • 621 Views
  • 0 replies
  • 0 kudos

Resolved! How to get ST60 B2370 Discovery Kit

I am looking for ST60A3 (B2309+B2310 or B1214+B2310 etc...)discovery kit in Taiwan.I try to find it on the official STMicroelectronics store, but I could not find any related information.How to buy ST60A3 discovery kit in Taiwan?

Sonialiu by Associate
  • 1077 Views
  • 2 replies
  • 0 kudos