Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STPMC1 - not writing configurations

Hello everyone.I'm currently building a controller for this energy measurement chip.So far, I've built my controller and can perform a remote reset and read data, but when I want to configure a register, I send my desired configuration, but when I re...

JEVelez by Associate
  • 1333 Views
  • 2 replies
  • 0 kudos

simple code for S2LP

Hello,Could you please provide a simple example source code to operate an S2-LP transceiver under the following conditions? My MCU is an STM32F103 connected via SPI1.A 25 MHz crystal is fitted to the S2-LP.External SMPS (1.8 V) is used.I want to tran...

About S2LP with STM32F103VCT

Hello everyone, I’m trying to control an S2-LP QTR via SPI1 on an STM32F103VCT. I completed the initial setup and configured the radio to 420 MHz. I then wrote a routine to transmit periodically, but I’m not seeing any RF output on the antenn...

SonDongSeong_0-1749466815822.png

L9663 Configuration

我的 L9663 SPI 无法正常工作,我想通过寄存器读取L9663的设备ID,但接收回来都是0XFFFF。我现在使用的MCU是STM32F103C8T6,以下是我的计划,希望大佬们帮我看一下有没有问题。

9ed9e1351aa588f1d3a73b2a1951397.png

STEVAL-IDP004V2 - "Error code 6148"

  Hi, please see attached screenshot. I'm experiencing a problem with the ST IO-Link Sensorkit and Master (STEVAL-IDP003V1/STEVAL-IDP004V2). I've connected the Master device via USB and used the TEConcept Control Tool as described in the ST instruct...

Screenshot 2025-05-26 115007.png
Jay6 by Associate II
  • 867 Views
  • 0 replies
  • 0 kudos

STHV748 Technical Support

Dear Manager.Hello, I am a student studying at a Korean university.I am developing a two-channel small ultrasound system.1. Try to use STHV748, a 4-channel pulser, as a pulsar, and don't use the other 2 channels. Should I connect to GND for channels ...

Resolved! STISO620 - pullup needed?

Hi to everybody and thank you in advance. I'm planning tu use the STISO620 as a function replacement for old-school optocouplers. STISO620 matches in every metric. My plan is use the part to interface an STM32 MCU.My application will detect falling e...

Tico_0-1748518314736.png Tico_1-1748518472569.png
Tico by Associate II
  • 1155 Views
  • 2 replies
  • 1 kudos