cancel
Showing results for 
Search instead for 
Did you mean: 

Signaling Line Circuit

ank2
Associate
Hi, The current design requirements for a Fire Panel system, demand power line communication over a distance of more than 1.2 km. More than 254 devices (detectors) would be interfaced to the main control panel. Suggest possible feasible solution for the above mentioned design specifications and share the relevant files. Also please specify the baud rate that would be maintained for the specified suggestions. Thanks.
1 REPLY 1
TDK
Super User

A differential signaling scheme like LVDS is going to perform best. A USAT signal over LVDS can work. Without repeaters, baud rate will be limited.

Perhaps read up on information already out there.

How Far, How Fast Can You Operate LVDS Drivers and Receivers? (ti.com)

If you feel a post has answered your question, please click "Accept as Solution".