Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BLUENRG change name "BlueNRG" doens't work

I have nucleo idb05a2 on board re401. i have compiled sensorDemo_BLEsensor-App. it work with Galaxy bluetooth 5.0 and not work with Honor bluetooh 4.2.Then i change name from "BlueNRG" to "TestBlue" (compiled and write) but still appired "blueNRG" st...

Wake up time S2LP-DK - - Low Power ?

Hello everyone,I have a small problem with my shield, the S2LP, when I start a transmission while waiting for an interrupt on my GPIO_0 (interrupt at low state), it sometimes never happens and my timeout is then called after 10 seconds, which is norm...

STM32F746ZGT6 to HDMI

Hi everyone, I'm working on a project where I interface the micro STM32F746ZGT6 with a CMOS sensor to acquire images. What I wanted to do is then transmit them using an HDMI connector but I don't understand which communication pins of the micro I cou...

LTurc.1 by Associate
  • 1419 Views
  • 2 replies
  • 0 kudos

Is there a tutorial or starter page to use the BlueNRG-M2 board? I'm not new to the STM32IDE or MX environment but it would sure help to see a tutorial first.

I'm using the BlueNRG-M2 connected to a Nucleo-L031K6 board. It looks like the V1.0 of the BlueNRG-MS software pack isn't compatible with my Nucleo board. I get an error when I try to download the BlueNRG-MS pack. Should I be trying a different on...

BlueNRG-132 Code development and debugging

Hi, I am new to the BlueNRG family and have been struggling to find the currently recommended development environment. I read that the STM32cube environment does not support it, so I have downloaded the last Atollic version (9.3). This does seem to s...

JHall.4 by Associate
  • 863 Views
  • 0 replies
  • 0 kudos