cancel
Showing results for 
Search instead for 
Did you mean: 

When OTA and bonding both features are enabled, the bond information gets erased from flash each time I disconnect from the device. Any suggestions on this?

Padmashree_NS
Associate II

I am using BLE Chat application where I have added the bonding feature. When I don't use OTA, I can connect to the device and bond it and the bond information stays even after reconnecting to the device.

But when the OTA is enabled, once I connect to the device and bond it and disconnect it the bond information is getting erased and the device is again asking to bond on reconnection.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0