Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Which WI-FI module to use?

Hello everyone!I'm planning to extend connectivity capaibility of my board where I use STM32f427 MCU, with WI-FI interface.Till now, I was looking for RN1810 and ESP32.Can you recommend me which WI-FI module is mainstream these days and easy to use?W...

DIvan.1 by Associate III
  • 916 Views
  • 1 replies
  • 0 kudos

BlueNRG issues with timers & low power modes

I'm having issues with the BlueNRG multifunction timers when using the sleep low power mode (SLEEPMODE_WAKETIMER). I've stripped down my project to create a minimal reproducible example which is described below.A virtual timer is being used to period...

mdmottola by Associate II
  • 1530 Views
  • 0 replies
  • 0 kudos

S2-LP EMC protection

Hello!Does the S2-LPQTR need a EMC protection on the Antenna (to protect RXp, RXn and TX)? I want to connect the Antenna with a SMA connector.

EmaEma by Associate
  • 665 Views
  • 0 replies
  • 1 kudos

How can use BLUENRG-M2SP with custom board?

Hello,I've developed a custom board with STM32F446 and BLUENRG-M2SP, but I can't realize connection. I use the same code for X-NUCLEO-BNRG2A1, in particular X-CUBE-BLE2 Sample App and I've changed SPI pin. If I set the UserBoard mode as HCI_interface...

AR1 by Associate II
  • 968 Views
  • 1 replies
  • 0 kudos

BLUENRG-2N does not work.

Communication with the chip BLUENRG-2N goes through SPI. When Chip Select GND, there is no interruption on IRQ line, all voltage and quartz are in order. Then I stitched through the SWD and the BlueNRG-1 ST-Link Utility program first with the BlueNRG...

Vandr.1 by Associate II
  • 1219 Views
  • 1 replies
  • 0 kudos