cancel
Showing results for 
Search instead for 
Did you mean: 

We want to use the S2-LPQTR for proprietary protocols. Therefore we need external control of the TX- and RX-mode of the transceiver. We intend to do this over GPIO 0 and 1, as short mentioned in the datasheet, page 65, table 61.

HOppl.1
Associate

Do you have a typical schematic or an application note that deals with such a setup, to have direct hardware control of the TX- and RX-mode, and also to access the TX and RX data in a very direct way?

In our application the TX/RX time and RX/TX time is critical and therefore we can't go over the FIFO with the data.

We are looking forward to your reply/suggestions - many thanks in advance.

Best regards,

Hanspeter

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0