Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! x-Cube-ST67W61 Package V1.1.0 Update for CubeMX

Dear All,I am waiting for the availability of the x-Cube-ST67W61 package update to version 1.1.0 which is available on GitHub but doesn't show up in CubeMX at the moment. Do you know when it will be available via embedded package update?Best regards,...

PKR by Associate
  • 445 Views
  • 1 replies
  • 0 kudos

S2-LP Transceiver interface with Antenna

Hello Community experts, I am working on my company's new product line designing about 10 products. We are planning to use S2-LP transceiver for 868MHz and 915 MHz devices. For at least 2 products, we need as long range as possible. Since the Half Wa...

ABSingh by Associate
  • 415 Views
  • 0 replies
  • 0 kudos

Resolved! ST67W61 pass-through mode

Hello, does ST67W61 module support pass-through mode?   I have an application based on a third-party IP stack and it would be a pain to rewrite it all with AT primitives. A far simpler solution would be replacing low-level calls to transmit and recei...

Resolved! X-CUBE-ST67W61 interface

  I am planning to have my application interface with the service API of the X-CUBE-ST67W61 Software package. How does the shell utility interface with the Service API? Is the communication interface through a queue?

X-CUBE-ST67W61 architecture.jpg

S2-LP: Minimal deviation for GFSK

Hi everyone!We are trying to launch the GFSK reception on S2-LP in the basic mode. We have noticed that by reducing the deviation to 10 kHz most of the received packets gets discarded and even those accepted have at least 2-3 bits of errors. This beh...

Resolved! ST67W611M1 wrong data received through SPI

Dear all, I'm trying to control ST67W611M1 wifi module by using a linux host chip. After flashing the newest firmware I reset the module to SPI mode. Some logs can be received through the uart interface and the SPY_RDY pin is drived to high level. Bu...

VL53L8CX I2C with ESP32

Hello,I wanted to share about the VL53L8CX sensor and it's I2C.I have been using a lot of VL53L sensors (5CX, 1X) and now the 8CX.It always used to work super easily but with the VL53L8CX I cannot seem to make it work. Running an I2C scan doesn't det...