Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

As part of the FCC/CE type approval measurements, every BT radio needs to be set in a constant transmit mode with modulation. How is this done with the BLUENRG-MSQTR?

Hi, We are having issues putting the BLUENRG-MSQTR on our board into the hci transmit test mode. We call the following two methods and they both return success but looking on a spectrum analyser, I don't see anything transmitted. ret = aci_hal_set_tx...

Moi by Associate
  • 1314 Views
  • 1 replies
  • 1 kudos

Resolved! Erase command timeout on BLUENRG-M2SP

I have a problem with a couple of BLUENRG-M2SP modules. I tried flashing the firmware under linux (We have to flash 100+ devices and each device needs a different firmware so plug and play flashing is not sufficient enough, so I copied ST's config fr...

DReib.1 by Associate
  • 1225 Views
  • 1 replies
  • 0 kudos

The I2C BlueNRG-1 always got 16 bytes.

Hi Friend,I used the I2C of BlueNRG-1 as slave to receive data. It always got 16 bytes, but my data is more than 16 bytes. The code snippet as follows. Could anyone help me? What's wrong with my code? I saw the data sheet said that I2C had 16-byte de...

TWu.6 by Associate II
  • 958 Views
  • 2 replies
  • 0 kudos