cancel
Showing results for 
Search instead for 
Did you mean: 

Can I use X-NUCLEO-BNRG2A1 with STM32F469 Discovery Kit?

Maurizio1
Associate III

Can I interface these two boards?

Can I program X-NUCLEO-BNRG2A1 without a Nucleo board? Is the X-NUCLEO-BNRG2A1 programmed via the host Nucleo board?

I'd like to not purchase the much more costly STEVAL-IDB008V2.

On the other hand, I'm just starting with embedded systems in general, so I'd like to avoid complications.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0