Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

how to set custom frequency for st7580 ?

Hi I am using NUCLEO-L053R8 with XNUCLEO- PLM01A1 board connected which is having ST7580. i am able to run the basic example given but now i wanted to change the Maximum central frequency which is in configurable as per the document *https://www.st.c...

0693W00000HpYlCQAV.png 0693W00000HpYoKQAV.png
ytriv.1 by Associate
  • 969 Views
  • 0 replies
  • 0 kudos

st7789h2 LCD MODULE issues

hello sir,My self-Mahesh firmware engineer Currently I am working with 1.54 inch display module(st7789h2),This module is configured with four wire SPI.I am facing some issues 1, Pixel writing is very slow. 2, Not able to control the brightness. 3, I...

MRedd.3 by Associate II
  • 8189 Views
  • 11 replies
  • 0 kudos

How IO-Link Works

Hello everyone,I have a board with STM32G4 and L6362 on it.But I have several questions about IO-Link itself.I want to know about sensor types on the IO-Link bus.If I want to make an encoder, what type of profile should define, or if I want to make a...