Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Implementation stack Bluetooth X-CUBE-BLE1 problem

Hi everyone,I try to implement the stack Bluetooth 4.2.0 X-CUBE-BLE1 with the sensorDemo application on a Nucleo-L452RE evaluation kit, coupled with X-NUCLEO-IDB05A1 Bluetooth Board.The code C has been generated thanks to STM32CubeMX 5.0.0 standalone...

SLAUR by Associate
  • 1295 Views
  • 1 replies
  • 0 kudos

BLUENRG devices firmware upgrade setup

Please help me with the setup required to flash the latest firmware version for the BlueNRG devices. I would request your help to explain me the setup required for both the usecases exlained below -There are some devices we have in stock and they nee...

Acharya by Associate
  • 797 Views
  • 0 replies
  • 0 kudos

Resolved! Sometimes I'm reading strange values for RMS voltage and current on my STPM32, but I do not know why. Is there something very special to concider?

Hello,I'm using a STPM32 to measure the ac line voltage and current. It is connected via a galvanic isolator ISO7341CDW to a STM32F072 with SPI. Most of the time, this works just fine. I can read the correct RMS values for I1 and V1 (Register DSP_REG...

SPIRIT-1 not always able to receive

Dear ST Community,I have the following test setup:- 1x SPIRIT-1 transmitter (reads a pin from a STM32 MCU and modulates it over the radio)- 2x SPIRIT-1 receivers (receive the pin state and pass it to the MCU)Expectation: Both receivers should receive...

VMeto.1 by Associate II
  • 666 Views
  • 0 replies
  • 0 kudos

How does UART work without the HAL layer ?

Title shortened in accordance with community guidelines.Original title: "How does UART work without the HAL layer? Does the shift register clear itself once it has transmitted its data? And what's the timing I need to have?"Some context, I'm using a ...

DTr.1 by Associate
  • 2130 Views
  • 3 replies
  • 0 kudos

Resolved! SPI Display Max resolution

Hi,I was looking at the display interface overview and saw that the max resolution for an SPI connection seems to be 480*272. https://support.touchgfx.com/4.19/docs/development/hardware-selection/hardware-components/hardware-selection-displayI'm curr...

DOkaz.1 by Associate II
  • 2687 Views
  • 2 replies
  • 0 kudos