Hi,I find the new chip STM32G0B1 from STM32CubeMX.And I want use this chip with SBSFU 2_Images.But I can not find the STM32G0B1 project from the X-CUBE-SBSFU v2.4.0.Is STM32G0B1 compatible with X-CUBE-SBSFU v2.4.0 ?How do I use STM32G0B1 with SBSFU 2...
Hi, I am trying activate read protection to level-1 with using batch(.bat) file. I am commanding to ST- Link Utility via batch file. My batch file code is like that:@ECHO OFF"C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Uti...
I'm trying to set the Read projection level to 1 after programming the application. Our manufacturing setup requires that we use J-Link rather than the ST-Link. I tried making a set of exit steps for the J-Link but it isn't working; I'm wondering i...
Hi,According to the document "AN5056-Integration guide for the X-CUBE-SBSFUSTM32Cube Expansion Package" Table 3. SBSFU code size reduction,In project "NUCLEO-G071RB", I build "1_Image_SECoreBin" by modify SECBOOT_CRYPTO_SCHEME from "SECBOOT_ECCDSA_WI...
I build Projects "NUCLEO-G071RB" in X-CUBE-SBSFU and load "SBSFU.bin" into the board.After reset the board, I download firmware "UserApp.sfb" with SecureCRT by using menu "Transfer > Send Ymodem" , but it failed.I also try to use "Tera Term", it dow...
I'm trying to build the SECoreBIn, and have changed the key (OEM_COMPANY_1) in:STM32CubeExpansion_SBSFU_V2.3.0/Projects/NUCLEO-G071RB/Applications/2_Images/2_Images_SECoreBin/Binary/OEM_KEY_COMPANY1_key_AES_CBC.binIf I have understood correctly from ...
I am working on STM32G030J6, and I programmed it using STMCubeProgrammer through BOOT0 pin. I have also changed the option bytes nboot_sel to 0 to boot from pin and NRST mode to GPIO. The code works fine when RDP level is set to 0. When RDP is set to...
FLASH memory protection is different between STM32G070 and STM32G071.But there is no stm32g070 in the sample project of x-cube-sbsfu package, only stm32g071.Based on project NUCLEO-G071RB, I commented out two protections and compiled them. I wonder i...