Resolved! Need support in developing audio application
I am trying to develop an audio application of my own using stm32f746g disco board.Can somebody share relevant documents which would be helpful for me to start from zero as i am a beginner?
I am trying to develop an audio application of my own using stm32f746g disco board.Can somebody share relevant documents which would be helpful for me to start from zero as i am a beginner?
I paid someone and she came up with a solution using STM32F103 and claims that it works for wav files using PWM and low pass filter with a digital attenuator. It didn't, and 1 year on I am still looking for the right MCU and the right solutionUM1642...
I am interested in developing Alexa built-in device using your solution mentioned in the Link.But this link also mentioned that "Amazon decided to maintain AVS for IoT system for existing products only. This solution can’t be used to develop a new pr...
Hello!For a week i've been trying to configure my stm32f302cbt6 and the tlv320aic3254 codec to trasmit data to the mcu through i2s_ext_sd but HAL_I2S_Receive returns 0s to the buffer although i see data coming out of the codec. I have configured i2s2...
Hi All,I want to start a project using TouchGFX, but it must also contain Audio Output on the headphone jack of my STM32F746G-DISCO board.I managed to get these two things to work separately: The TouchGFX part using TouchGFX Designer, and the Audio O...
Hi all,I am using a STM32H7 and I implemented a composite usb device (CDC + AUDIO recording) using IAD interface descriptor.I can successfully configure the audio interface as type I PCM (I tested both 16 and 32 bit), but if I try to configure the au...
I'm trying to receive SPDIF data using an STM32F446RET using PB7 as SPDIFRX. The signal itself is perfect, a clear and sharp waveform can be seen directly at the input pin. The whole stuff is configured in CubeMX which also generated the code for int...
If anyone is familiar with Digital Audio Workstations (DAW's), you can then select the type of audio input device in the application, to then choose which channel to monitor and record.I'm familiar with the process of how to record the incoming audio...
I'm stuck. I'm able to send a 440 Hz sawtooth wave to output over USB from Nucleo board (device) to my computer (host).The only problem is, there's this repetitive clicking / choppy sound in the resulting audio when I record with Audacity. The click...