Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STISO620 - pullup needed?

Hi to everybody and thank you in advance. I'm planning tu use the STISO620 as a function replacement for old-school optocouplers. STISO620 matches in every metric. My plan is use the part to interface an STM32 MCU.My application will detect falling e...

Tico_0-1748518314736.png Tico_1-1748518472569.png
Tico by Associate II
  • 83 Views
  • 2 replies
  • 1 kudos

Resolved! Is L7987 Synchronous or Asynchronous?

Hi all,I am designing a 48 volt to 12 volt 3 amp DCDC asynchronous buck converter (with frequency > 200kHz) and I found the L7987. Although it says asynchronous in the datasheet, it looks like synchronous in the block diagram. I am confused, can some...

AziD32 by Associate
  • 204 Views
  • 3 replies
  • 0 kudos

Need technical guidance for SCLT3-8BT8

I need to interface Digital input sensors of PNP & NPN type both in one of my product.Can I use SCLT3-8BT8 to interface both the type of sensors? Ho should we detect high side & low side through SPI lines on microcontroller?Thanks for your help in ad...

NDesh.2 by Associate II
  • 62 Views
  • 1 replies
  • 1 kudos

Sub1GHz module

Hi, I would like to explore the possibility of using the sub1GHz product solution from ST, particularly, the part number S2-LPTX.Here are the requirements1. We need One Receiver and 4 Transmitter (as shown in the image) which are operating at 433MHz ...

AshnoJames_0-1748435550932.png