2024-03-18 2:44 AM - last edited on 2024-05-08 8:33 AM by Amel NASRI
I'm experiencing a problem with the ST IO-Link Sensorkit and Master (STEVAL-IDP003V1/STEVAL-IDP004V2).
I've connected the Master device via USB and used the TEConcept Control Tool as described in the ST instructions. Everything went smoothly up to step 6/7 according to document UM2232. However, from this point onward, I'm not receiving the expected data from the sensor. Instead, I'm getting the message "Invalid Data," preventing me from plotting any data.
Could it be that the sensor needs further configuration?
Or is there perhaps a write protection or similar feature that needs to be deactivated?
Could there be a malfunction with the Sensorkit?
I've checked the setup:
I would appreciate any assistance in resolving this issue.
2025-05-26 3:54 AM
Hi,
I am experiencing the same problem. did you get to the solution?
Thanks,
Jay
2025-06-02 2:28 PM
Hi Jay,
I'm sorry, I didn’t end up working on the problem, as the project was closed before I got to it.