STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! HAL interrupt function

Dear @KDJEM.1 Whenever, I implement the HAL_Interrupt functions(say HAL_UART_Receive_IT();). What is happening at the backend, to use those interrupt function I should enable the global interrupt (NVIC) in CubeIDE. What are these global interruptsals...

ajimathew by Associate III
  • 6482 Views
  • 5 replies
  • 6 kudos

Loading WAV file with CubeProgrammer

I need to load a few small audiofiles to the flash memory of STM32F407VGT6 on my F4Discovery board and now I am curious about one thing. Is it possible to load WAV samples with STM32CubeProgrammer?For example, if I use xxd command in Ubuntu to conver...

bug in stm32cubeProgrammer version v2.13.1

Hi, I found a bug in stm32cubeProgrammer version v2.13.1. When you try to readout unprotect an STM32H7A (without smps) and if its rdp level is set to 1, that didn't works. I have to unlock it manually inside my software.  

Nnabb.1 by Associate II
  • 957 Views
  • 0 replies
  • 0 kudos

Resolved! STM32CubeProgrammer 2.13 bugs

Hello,STM32CubeProgrammer 2.13 has some bugs:See attached picture, the Target information does not report the correct flash size, although it is reading the memory size correctly at 0x1FFF75E0Why does it have to read multiple times in a row the same ...

Kraal by Lead
  • 9791 Views
  • 11 replies
  • 2 kudos