STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

UART interface programming speed

Hello all,I'd like to know if there is a set of acceptable UART baud rates for CLI use (CubeProgrammer CLI defaults to 115200 baud for UART).Looking at the GUI for CubeProgrammer, after selecting UART, it shows that a baud of 460800 or 921600 is poss...

shortnr by Associate
  • 4117 Views
  • 4 replies
  • 1 kudos

Resolved! Programming to external flash on STM32U5A9J-DK fails after around 2.5 MByte. How to fix this?

I'm using a STM32U5A9J-DK with TouchGFX. Smaller projects work just fine. But aufter integrating an Animated Image (approx. 37 MBytes of assets), the programming fails. The console log is as follows:STMicroelectronics ST-LINK GDB server. Version 7.3....

JWill.11 by Associate II
  • 7578 Views
  • 11 replies
  • 0 kudos

Anyone successfully using Cube Programmer C++ API?

Haven't found anyone talking about the new API here. I'm trying to code a program that flashes a STM32F334, reads processor's UID and post it to a proprietary database. STM32CubeIDE and CubeProgrammer works fine. I also managed to run C++ API and ide...

VMüll.1 by Associate II
  • 10263 Views
  • 17 replies
  • 1 kudos

Resolved! Flash Memory program

Dear @KDJEM.1 when I read the manual "rm0432" It is given thatThe Flash memory programming sequence in standard mode is as follows:1. Check that no Flash main memory operation is ongoing by checking the BSY bit in theFlash status register (FLASH_SR)....

flash.png
ajimathew by Associate III
  • 2300 Views
  • 1 replies
  • 1 kudos