cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, I try to install STM32CubeProgrammer_2.10.0 on linux RH. Installation is OK but when I run I have error messages : on RH 7.8 is with GLX 1.2 version (because we must have 1.3 or >) on RH 7.9 (with GLX 1.4) Exception in Application start method

PLECU.1
Associate II

In RH 7.9 , Exception in Application start method (java.lang.reflect.InvocationTargetException)

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Sara BEN HADJ YAHYA
ST Employee

Hello @PLECU.1​ ,

Could you please provide us with more information about the PC environment (processor, architecture... ) ?

Thanks,

Sara.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
PLECU.1
Associate II

Hi Sara ,

It's a virtual Linux Red Hat machine in RH 7.8 .

Processeur Intel Neon 2,2 Ghz architecture x86_64

RAM : 32Gbs

Tanks for your help

PLECU.1
Associate II

Hi ,

I have testing installation on a new directory (with "root" account)

Installing is well , running STM32CubeProgrammer open the IHM (without possibility to resize the window) but when I want to run it from my $HOME (with my account user) , it doesn't open .

How can I run the installer (root or user ?) and run IHM STM32CubeProgrammer correctly (for all users) ?

thanks