User Activity

I am using an STM32H757. I understand how, using the TrustedPackageCreator and an HSM, I can supply our manufactures with an encrypted version of the firmware and limit the number of product instances they can produce. My question is, when the produc...
Connections:D- = PA11D+ = PA12and Gnd to GndAs well, Boot0 is connected to VDD. I have nothing connected to the UARTS or CAN.Even with this setup, upon reset, the system runs the code I have downloaded (via ST-Link) rather than the bootloader. I th...
Kudos from