2022-08-12 4:51 AM
Hi.
I'm developing with custom board which has a custom QSPI (EN25QX128A - 16Mbytes flash), so I need to make an external loader used by STM32CubeProgrammer.
First I wrote a code that interacts with QSPI and it works fine.
So I changed this code to fullfill the external loader specification.
But when I connect the target board by clicking "Connect" in STM32CubeProgrammer, I checked that "Init()" is called but SystemClock_Cofnig() fails.
I tried to change clock-setting in various ways, but still get stuck in Error_Handler.
What am I missing working with External loader?
Please help me to get out of this trap.
Thanks.
Solved! Go to Solution.
2022-08-12 5:38 AM
Perhaps that the clock / pll is already running?
Check the local/auto variable is cleared.
USART cam be used for diagnostic output.
System can run from HSI.
2022-08-12 5:38 AM
Perhaps that the clock / pll is already running?
Check the local/auto variable is cleared.
USART cam be used for diagnostic output.
System can run from HSI.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.