STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! CubeProgrammer reports RDP over native USB

When plugging in a device in DFU mode to a native USB port of the notebook cubeprogrammer reports:When using it over USB HUB or other port the Cubeprogrammer works fine (we never activated RDP).USBDeview shows no difference in the installed drivers. ...

0693W00000aISk7QAG.png
tguly.1 by Associate III
  • 6392 Views
  • 7 replies
  • 0 kudos

Resolved! hex (or bin) file to elf using Cube Programmer

Hi all.With build project I can obtain .bin, .hex and .elf file.I need to manipulate the file to add a CRC in determinate position. SO I use .bin (easiest), then convert in .hex and .elf file using:arm-none-eabi-objcopy -I binary -O ihex --change-sec...

TheRaprus by Associate III
  • 5563 Views
  • 3 replies
  • 0 kudos

No ST-LINK detected

I have got an Nucleo L073RZ   ( and also a discovery 407,F410RB and 4 more nucleo boards) .   It is a new board just unboxed .  I can see it as a drive  in my computer beside disks  so I know it is working.   But st link cannot detect it.   All my  b...

Resolved! Please hint me on how to program with ST-Link

Dear ST I tried to connect with MCU "stm32l07x using STM32CubeProgrammer as below image 1, image 2. Board power is 3.09V to be measured by ST-Link.However, I can't program it.  carefully check the st-link pin maps as VCC(#1), SWDIO (#7), SWCLK(#9), R...

kevin1971_1-1700453285443.png kevin1971_0-1700453258263.png
kevin1971 by Associate II
  • 2593 Views
  • 5 replies
  • 1 kudos

CubeProgrammer error on STM32U545

Hi, I've developed a custom ExternalLoader for STM32U575VGT6Q installed on my board, following the online guides provided by ST, obtaining a fully functional version. On the new version of the board I have an STM32U545VET6Q, so in ExternalLoader proj...

ReadProcedure.png
Pc10 by Associate II
  • 15937 Views
  • 23 replies
  • 3 kudos

Resolved! change DBANK unchecked to checked

Hi, I am a beginner in STM32L4. I set DBANK unchecked accidentally in STM32CubeProgrammer on STM32L4S7ZIT6. Now I want DBANK to be checked, but I don't know how to do. I try check DBANK and apply, but fall. It give me 2 errors. (after read, the DBANK...

alyssa_0-1699603330766.png alyssa_1-1699603458360.png alyssa_2-1699603474874.png alyssa_3-1699603743354.png
alyssa by Associate III
  • 1500 Views
  • 1 replies
  • 0 kudos