STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32H747I-DISCO Flash Example

"DCMI_SnapshotMode DCMI Snapshot Mode example"I am a beginner and would appreciate help with the following Readme.txt:"In order to make the program work, you must do the following :- Open your preferred toolchain- For each target configuration (STM32...

Programming Metadata on eMMC with lower address

Hello,I am doing some programming with the STM32CubeProgrammer. The metadata is programmed as follow:   P 0x06 metadata1 Binary mmc0 0x69000 metadata.bin   The tool returns an error because the expected address is *NOT* 0x00080000....

MToum.1 by Associate II
  • 1618 Views
  • 1 replies
  • 0 kudos

STM32CubeProgrammer DFU instable

Hi,our c 13:26:59 : STM32CubeProgrammer API v2.14.0 | Windows-64Bits 13:27:37:380 : UR connection mode is defined with the HWrst reset mode 13:27:38:416 : Device Descriptor: 13:27:38:416 : |_bLength : 0x12 ...

JBurg.5 by Associate II
  • 3272 Views
  • 4 replies
  • 1 kudos

Resolved! CubeProgrammer and QT dependencies

Hi,I've just downloaded the STM32CubeProgrammer software in order to build a C++/QT project with it.As I was adding the CubeProgrammer_API.dll into my project, i found that i needed some QT5 dlls dependencies such as : Qt5Core.dll Qt5Script.dll Qt5Se...

Sofiane by Associate II
  • 3553 Views
  • 3 replies
  • 3 kudos

STM32CubeProgrammer way too long to load

I updated my old STM32CubeProgrammer to 2.14. Now it  takes a very long time to start... Much more than the time to program the MCU! What is he doing during this time? No doubt marketing exchanges with ST servers. The primary use of this type of tool...

stm32programmer is not connecting with device(STM32G0)

Hello forum,we are facing a very strange issue with the STLINK-V3MINIE debugger.Controller: STM32G0B1CE seriesSTMprogrammer version: 2.14.0Debugger:  STLINK-V3MINIEwe are trying to connect the device(controller) with the stm32programmer application u...

image (3).png image (4).png
Dthum.1 by Associate III
  • 3699 Views
  • 3 replies
  • 0 kudos

Resolved! How to use STM32CubeProgrammer over CAN Bus?

Hi, are there any information's or app-notes available how to use this programmer over CAN bus. I cant find any information which hardware is supported or how make the can hardware on my laptop visible to the programmer. Thanks for your support!

MKemp.1 by Associate
  • 5382 Views
  • 3 replies
  • 0 kudos