STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Can't down STM32Cube Programmer

Hello,I have been trying to down the STM32Cube programmer but I reach a point where nothing happens. I have tried this on 2 different  browsers on 2 computers and the same thing happens.I go to the site https://www.st.com/en/development-tools/stm32cu...

nkyriakou_0-1702393199552.png

Resolved! Need help with programming STM32H563 using UART

I had created a project in STM32CubeIDE for the STM32H563 chip. I was able to flash it through UART1 using STM32CubeProgrammer but the code seems not executing. The code is just to toggle a LED every 500ms   int main(void) { /* USER CODE BEGIN 1 */...

Resolved! STLink V2 Not recognizing STM32CubeProgrammer?

 ST Link not recognizing STM Cube Programmer? - From screenshot you can see NO ST Link detected in serial number drop down and has no target information. I can (and did) upgrade firmware, On doing so, it's throwing following error( ST-Link device los...

Screenshot 2023-12-12 140310.png

ST_Link V3MINI and Cube programmer

Dear mr.I'm having problems with my project,Everything was working fine, but one morning I lost connection with the target unit, see attached image.I tried this with:  Two ST_Link V3MINI (I got them directly from ST)  Three different target board STM...

Micisag by Associate
  • 2319 Views
  • 3 replies
  • 0 kudos

STM32g474 processor nSWBOOT0 default option byte

We want to update the software of STM32G474 processor via uart. However, when we look at the "Pattern 14" option in the bootloader settings for this processor, the "nSWBOOT0" option byte is requested to be 1. However, we see that the default setting ...

mcelik by Associate
  • 1925 Views
  • 1 replies
  • 0 kudos

Resolved! STM32_Programmer_CLI.exe question

I have a custom board with STM32G070RB micro. I programmed the board several times for debugging in the development phase using theST-LINK//V2 in CubeIDE.Now I would like to generate a .bat file to program the boards, but I am facing some problems.My...

tabekb by Associate III
  • 17800 Views
  • 14 replies
  • 4 kudos

CubeProgrammer Static library files

Hi, I'm trying to use the cubeprogrammer api in my win32 application for firmware update. I'm able to do this, but there's a lot of .dll files that are required and it clutters the entire project. Is there any way you can provide a static .lib (code ...

Snapark by Associate
  • 999 Views
  • 0 replies
  • 0 kudos

Stm32 programmer external loader delay

I have been using custom external loader for a long time without any problems. I noticed a problem when I tried to upload to a board without an external flash ic. I am using CLI 2.14.0. While mass erase completes in a few seconds under normal conditi...

Okeskin by Associate III
  • 1418 Views
  • 1 replies
  • 0 kudos