2023-03-16 8:30 AM
I have attached the log output of the Programmer. Device enters DFU mode correctly and it is being recognised by windows but as soon as a connection attempt is done, the device resets after some time. Any way that I can debug the bootloader code and check what is going wrong?
The chip used is : STM32F401CCU6
And the binary available on the System memory is attached below which might tell what version it is.
Edit:
1- Added the chip version
2- Attached the hex of the system memory
2023-03-17 7:49 AM
Hello @NMich.3,
Could you specify the part number as well as the bootloader version of your device ?
Thanks,
Aziz
2023-03-17 12:22 PM
Hi @NMich.3
The forum moderator had marked your post as needing a little more investigation and direct support. An online support case has been created on your behalf, please stand by for just a moment and you will hear from us.
Regards,
Billy
2023-03-18 4:04 PM
I've not flashed the bootloader my self. Is there a way to get the version of it out from the Stm32Programmer?
When I compare the flash addresses from the System memory with another device where DFU mode functions correctly, there is not difference.
I would also like to mention that programming the device over JTAG works just fine.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.