STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32 cube programmer

Hello everyone,I am trying to connect device with stm32  cube programmer vai UART connection I am not able to connect initial but as some resource form st community and other online article I able to connect but it not able get into application is th...

PESHWA by Associate II
  • 2794 Views
  • 6 replies
  • 0 kudos

API: STLink detected but cannot be connected to.

I want to use the STM32CubeProgrammer C++ API to do high-speed real-time automated debugging (i.e. use it as an oscilloscope). I used as a basis the Example_2 given in the API's documentation. The STLink is detected since I can get info from it which...

_legacyfs_online_stmicro_images_0693W00000bjDGPQA2.png
AMabi.1 by Associate III
  • 3844 Views
  • 7 replies
  • 1 kudos

cube programmer - leave dfu

hi in the previous tool DFude v3.0.6 we had a button called -leave dfu mode,that button made disconnection and reset to MCU if you were connected with USB, so after flashing the MCU jump to application FW,now in the cube programmer, we don't have thi...

NBita.1 by Associate II
  • 2061 Views
  • 1 replies
  • 1 kudos

ST-Link v2 Cube programmer

Hi all, new to this. I am trying to remove read and write protection. In the option bytes, I cannot change wrp-0 and wrp-1. The progress bar on the lower part of the gui says 100% but does not actually finish. when I check the live update box, I get ...

LesterC by Associate
  • 1335 Views
  • 2 replies
  • 0 kudos

Resolved! Why might setting BFB2 cause printf to stop working?

I've written a fairly simple test case for using the system bootloader to boot from flash bank 2 on a STM32F429ZIT6U (developing on a Nucleo F429ZI board). With stdio redirected to a UART, I'm able to direct the code to:Mass-Erase Bank 2Copy the ent...

Brian H by Senior
  • 8273 Views
  • 14 replies
  • 0 kudos

Programmer CLI - safety lib - <pattern> parameter

We are using the safety lib (-sl) command with X-CUBE-STL library. Without <pattern> parameter, it is working. When trying to use 0xFF for <pattern> parameter, generated .elf is not even valid and cannot be loaded. Is there a workaround for this?For ...