Skip to main content
Amelie ACKERMANN
ST Community Manager
April 16, 2026

[Coming June 2026] Raspberry Pi support for STM32CubeProgrammer

Related products:STM32 software tools
  • April 16, 2026
  • 19 replies
  • 9438 views

Native Raspberry Pi support is coming to STM32CubeProgrammer, and it’s driven by your feedback.

With STM32CubeProgrammer v2.23, scheduled for June 2026, ST will introduce a Linux Arm 64-bit package available on st.com, enabling STM32 programming directly from Raspberry Pi platforms.

This new package allows you to fully leverage 64-bit Raspberry Pi platforms, including:

  • Standard models (flagship) series: from Raspberry Pi 3B to Raspberry Pi 5.
  • Zero (compact form factor) series: Raspberry Pi Zero 2 W.
  • Compute models (industrial & embedded) series: from Raspberry Pi CM3 to Raspberry Pi CM5.

What will be supported?

This first Raspberry Pi release supports all STM32 devices and core programming features:

  • Internal and external flash programming
  • OTP programming
  • Option bytes configuration
  • RDP regression with password (for supported products)

This provides a reliable way to program STM32 devices using a Raspberry Pi–based setup.

Interfaces and connectivity

All existing STM32CubeProgrammer interfaces remain supported and unchanged, including:

  • ST-LINK (SWD/JTAG)
  • J-Link
  • UART
  • USB
  • Bootloader via ST-LINK V3

In addition, this release adds direct GPIO-based SPI and I2C communication, allowing Raspberry Pi systems to connect straight to STM32 bootloader interfaces, without external debug hardware such as ST-LINK V3.

What will not be included in this release?

To keep the package lightweight and optimized for Raspberry Pi:

  • No GUI
  • No debug features (SVD files removed)
  • No debug authentication support
  • No secure firmware install (SFI)

Supported operating systems

  • Raspberry Pi OS (Debian 12 “Bookworm” or later)
  • Ubuntu 22.04 LTS or later

Why this matters

This release enables easier integration of STM32 programming into automation, CI/CD, test benches, and remote maintenance workflows using Raspberry Pi, now with an officially supported toolchain.

We are also aware that some programming service providers and integrators also use Raspberry Pi in their flows. This new package offers them a standardized and supported way to run STM32CubeProgrammer on Arm-based platforms.

The download links and documentation will be shared on st.com and the ST Community as soon as the v2.23 release is available in June 2026.

In the meantime, feel free to use this thread to:

  • Tell us how you plan to use STM32CubeProgrammer on Raspberry Pi
  • Share which additional features would matter most to you in future updates

Thank you again for your continuous feedback and for driving the evolution of our tools.

Additional resources

First published on Apr 16, 2026

19 replies

Andrew Neil
Super User
April 16, 2026

Is this going to be just Raspberry Pi, or would it work on other ARM Linux platforms running Debian  or Ubuntu ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
April 16, 2026

(never mind)

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Maxime_BELAVAL
ST Employee
April 16, 2026

Hello Andrew, good question actually.

This developer news highlights Raspberry Pi support, which has been requested since 2019.

However, this new package is built for aarch64 platforms so it is not limited to Raspberry Pi only.

Max

Associate
April 16, 2026

Super duper!

I hope it will work on the STM32 Linux offerings as well in the future!

Associate III
April 17, 2026

It could be a reliably programmer for our integration tests of libraries and drivers running on a pi with a couple of boards connected.

Visitor II
April 23, 2026

Why not also for the RPi pico?

Kazimierz Król
Associate III
April 23, 2026

From the title I thought we would be able to program Raspberry Pi using STM32 Cube Programmer :)

Andrew Neil
Super User
April 23, 2026

@BWH "Why not also for the RPi pico?"

Because the RPi pico is just a Cortex-M0 microcontroller - not a Linux computer!

 

There are plenty of articles on using the RPi Pico to make an SWD debug probe; eg,

https://mcuoneclipse.com/2023/04/08/open-source-picolink-raspberry-pi-rp2040-cmsis-dap-debug-probe/

https://visualgdb.com/tutorials/raspberry/pico/picoprobe/

but that's a completely different topic.

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate III
June 25, 2026

I hope Raspberry Pi support Releasing by this Weekend.

Visitor II
June 30, 2026

It seems that version 2.23.0 has been released, and the newest version of UM2237 describes the installation process. However, the arm64 deb is not available to download.
When can we expect it to be made available?
 

 

Associate III
June 30, 2026

In My case it shows , 5 options : 

Will this supoorted Older version of Raspberry Pi Model like 3B.