STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Firmware Upgrade failed CubeProgrammer_API

I am testing firmware upgrade API from CubeProgrammer_API. For some reason, it keeps printing that the firmware upgrade failed, but when i check the firmware version of my device, the firmware has been updated. Does anyone know what is the cause of i...

i124q_0-1710863192582.png
i124q by Associate II
  • 1808 Views
  • 3 replies
  • 0 kudos

Resolved! DFU error using CubeProgrammer_API

I am working on implementing a firmware update on my electron app using CubeProgrammer_API. I keep encountering issues on connecting to the DFU bootloader in which is giving me CUBEPROGRAMMER_ERROR_NOT_SUPPORTED (-5). I compiled my code into a .exe a...

i124q by Associate II
  • 1385 Views
  • 2 replies
  • 1 kudos

Resolved! STM32CubeProgrammer External Loader Partial Page

Hello, I have made a custom external flash loader(.stldr) file for my STM32 based board. Reading the content of the external flash via CubeProgrammer works fine. But when programming i run into the following problem: CubeProgrammer tries to write par...

CRich.4 by Associate III
  • 5107 Views
  • 10 replies
  • 2 kudos

Resolved! X-NUCLEO-LPM01A board not found on Windows 10 or MAC

i've installed versions of STM32CubeProgrammer on my windows 10 PC as well as my MAC....i'm following the instructions in um2269 (section 8) on updating firmware, but see a message saying "No DFU detected" under the USB configuration panel....  selec...

biosbob by Associate
  • 1702 Views
  • 1 replies
  • 0 kudos