STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Troubleshooting CUBE Programmar Settings Change Error

I briefly changed the option byte setting through CUBE ProgrammmerIt was changed well before, but I tried to change the DMEP setting and return it because I couldn't want it, but an error occurred and it is not changing The error appears as follows, ...

04.JPG
ark2 by Associate III
  • 956 Views
  • 0 replies
  • 0 kudos

Multi Board Programming

Hi,I have 20 boards in a 4x5 panel board. all boards have the same MCU. is it possible to program all boards via a panel at the same time? if so, how can I do that? which software and hardware tools do I need?Thank you.

mehmetk by Associate
  • 1553 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 cube programmer locks in automatic mode

Automatic mode works fine just to download binaries to the MCU.If It try to set option bytes read out protection to BB afterwards, the software will lock.It displays:15:20:13 : UPLOADING OPTION BYTES DATA ...15:20:13 : Bank : 0x0015:20:13 : Address :...

Alex. M by Associate
  • 3557 Views
  • 5 replies
  • 1 kudos

[Feature Request] Cubeprogrammer address section

Hello,I have a feature request for the STM32CubeProgrammer.As we know, when we connect the board, we can display the memory fields as like following:But when I disconnected from the board, the fields are gone:I know that this is not a bug, its a feat...

mcagriaksoy_0-1711093050768.png mcagriaksoy_1-1711093073833.png mcagriaksoy_2-1711093232799.png