STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Error: Problem occured while trying to connect

STM32CubeProgrammerを使用してボードをConnectしようとしたがErrorが発生する。使用しているボードはSTM32F746です。STM32cubeideでプロジェクトをRunした後にDebugをしなかった後にこのような動作が発生するようになりました。ジャンパーピンは5Vlinkに接続しUSBにてPCと接続しています。対処法を教えていただきたいです。

shoya88 by Associate
  • 1623 Views
  • 1 replies
  • 0 kudos

STM32WL5 full chip flash failing

I am using a Wio-E5 mini devboard by Seed-studio and an ST-Link/V2 to program it.After setting the Read Out Protection to AA, I was able to read and write from and to the memory and do a mass erase.However, programming from CubeIDE always failed. I w...

FMS_1-1712932177164.png FMS_2-1712932220008.png FMS_3-1712932316483.png FMS_4-1712932415318.png
FMS by Associate
  • 1124 Views
  • 0 replies
  • 0 kudos

Any NAND flash examples for External loader?

I failed to make the .stldr for a NAND flash. I have followed the steps of initial System CLK, GPIO, NAND, and then Erase&Write the chip. Unfortunately, nothing wroted into the flash.The open resources are more about SPI/QSPI. It is helpful if ther...

Czhu.1 by Associate
  • 2066 Views
  • 3 replies
  • 1 kudos

Resolved! STM32 Cube Programmer

Hi,I want to load a program so that when I unplug from computer and plug it again it is still running. To load the binary, I am using STM32 Cube Programmer. The program is correctly running, but when I click on the "Disconnect" button it stops runnin...

Alberto4_0-1712825901865.png
Alberto4 by Associate II
  • 4327 Views
  • 8 replies
  • 3 kudos

STM32CubeProgrammer 2.16 - cannot program MCU by USB

Hello,After installing STM32CubeProgrammer v2.16, I was unable to program a STM32F412 by USB (in DFU mode).I've never had a problem doing this and after uninstalling v2.16 and installing v2.15, everything worked fine.This problem was also confirmed b...

STeve-o by Associate
  • 2083 Views
  • 3 replies
  • 0 kudos

STM32CubeProgrammer 2.16.0 crashing in SWV

Hello,I'm using STM32CubeProgrammer version 2.16.0. The debugging works fine, but if the connection with the target is lost or probably some bad message is received on the client side, the application crashes. So in the first place I can't even see t...

krasl by Associate
  • 1009 Views
  • 0 replies
  • 0 kudos

CubeProgrammer 2.16 CLI problem - warning

After upgrading CubeProgrammer to new release 2.16 CLI commands started to fail during verification phase when changing option bytes on STM32U5A5. Sample command which fails:STM32_Programmer_CLI -c port=SWD mode=UR --hardRst -ob WRP1A_PSTRT=0xff WRP1...

TDJ by Lead
  • 1145 Views
  • 1 replies
  • 0 kudos