cancel
Showing results for 
Search instead for 
Did you mean: 

how can i pass step 7 while setup stm32 cube programmer

Gdönm.1
Associate II

when i create this program everything is ok until step7. however i cant pass step 7

and window is below.0693W000008xUekQAE.png

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Houda GHABRI
ST Employee

Hi @Gokhan dönmez​ ,

To be honest it is the first time we see this behavior :) .

Just to be sure, can you confirm if you install the STM32CubeProgrammer tool using these steps:

  • Download STM32CubeProg-Win-64bits zip package (64bits because you are using win10 (64 bits))
  • Extract the zip package
  • Execute SetupSTM32CubeProgrammer-vx.y.z.exe (Run as admin ) ,which guides you through the installation process.

Houda

View solution in original post

13 REPLIES 13
Houda GHABRI
ST Employee

Hi Gdönm.1

Can you please tell more informations :

  • which CubeProgrammer version you are using?
  • Which OS you are you using, is it on Windows?

Houda

Hİ Houda Ghabri,

Sure ,

i m using version 2.7.0 CubeProgrammer

I m using win10 (64 bits).

Thanks for answer.

Gokhan.

Houda GHABRI
ST Employee

Hi @Gokhan dönmez​ ,

Can you please try to install CubeProgrammer with admin rights in new folder and tell me if it is OK?

Houda

Gdönm.1
Associate II

Hi Houda Ghabri

I tried to install Cubeprogrammer with admin rights in new folder now but i don't install it.

Gokhan

Houda GHABRI
ST Employee

Hi @Gokhan dönmez​ ,

To be honest it is the first time we see this behavior :) .

Just to be sure, can you confirm if you install the STM32CubeProgrammer tool using these steps:

  • Download STM32CubeProg-Win-64bits zip package (64bits because you are using win10 (64 bits))
  • Extract the zip package
  • Execute SetupSTM32CubeProgrammer-vx.y.z.exe (Run as admin ) ,which guides you through the installation process.

Houda

Houda GHABRI
ST Employee

Hi Gdönm.1,

I'm coming back to see if it works for you since my last answer.

I hope so :)

Houda

AI1
Associate II

Hello,

I am having the same problem , I tried above steps and nothing changed.In step7 I can't pass this step.

If you have found the reason, could you please share it!

Thanks .

0693W00000LyaBxQAJ.png

KUçan.1
Associate

Hi I have the same issue, I tried to load it to a different folder with admin rights as you said but it didn't work. Have anybody solved it?

What if you do NOT enable creating any shortcuts on a previous step?