STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32H7 and FLASH Loader Demonstrator

Recently I've download and installed Flash Loader Demonstrator v 2.8.0 and It turned out it doesn't support STM32H7 microcontrollers. Project I working on requires programming software using UART2 communication port. Flash Loader is able to connect w...

Use Flash Loader with  a STM32L471 512K

Posted on September 13, 2017 at 13:25Hi,We are developed a proyect with teh MCU STM32L471. We have downloaded the appliacation Flash Loader V2.9  but don't have the file .STMap for this MCU.We have a questions:- Is there a newer version of the Flash...

STM32Cubeprogrammer, STM32H7 and IWDG1

Posted on July 16, 2018 at 16:12Hello,for the H743, the Stm32CubeProgrammer  lists Option-Bytes->User Configuration->IWDG1 as 'Unchecked: Controlled by software' and 'Checked: Controlled by Hardware'. However the meaning is inverted! With IWDG1 unch...

STM32CubeProgramer connecting to STM32H753IIK6

Posted on July 12, 2018 at 01:45I'm having trouble getting the STM32CubeProgramer to connect to my STM32H753IIK6 chip using the serial port when going into boot loader mode. I'm using RESET and BOOT pins to get the chip into boot loader mode but the...

Using FatFS R0.12c with STM32CubeMX

Posted on June 08, 2018 at 03:47I followed in the instruction https://community.st.com/s/feed/0D50X00009bMM8bSAG , but it doesn't work for me. I am using the SD card with FreeRTOS with the DMA configured. Code is generated with STM32CubeMX. I am usi...

cleonb322 by Associate III
  • 2322 Views
  • 3 replies
  • 0 kudos

STM32 DFU cross-OS support

Posted on May 27, 2018 at 00:38I'm working with the Nucleo F767ZIT (QFN-144) to test the F7's abilities, and currently I'm struggling with the USB DFU capability. I've read a few posts about issues getting the DFU working due to the F7 requiring opt...

STM32CubeProgrammer CLI lack of options

Posted on March 15, 2018 at 16:101. How to specify to which one ST-link to connect using CLI? In the ST-link utility we had an option to specify a serial number. How to do it with a new STM32CubeProgrammer? I have tens of ST-links connected on the s...

ri by Associate II
  • 2708 Views
  • 4 replies
  • 0 kudos

STM32CubeProgrammer with DFU erase error

Posted on May 01, 2018 at 22:20I recently started using the STM32CubeProgrammer for flashing MCUs via their DFU bootloader in the system memory. (After resolving the windows driver conflict with DfuSe, the lesson is: use Zadig instead of the batch f...

Ben K by Senior III
  • 1369 Views
  • 0 replies
  • 1 kudos