STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

stm32WB. How to reset to factory settings?

Hello,  I have a problem with the return of the STM32WB to the factory settings  When I use the next command  STM32_Programmer_CLI.exe -c port=SWD -w32 0x5800040C 0x00008000 that looks like that  But finally, when I read FUSE I saw that Stake was no...

08bf8040-d86f-4e8c-8268-a610e0253820 (1).jpeg FUS.jpg
Ronil by Senior
  • 1979 Views
  • 1 replies
  • 0 kudos

Resolved! Updating STM32F373 over USB DFU Fails to Connect

I'm able to connect to my STM32F373 board over a USB virtual port com successfully.  I'm also able to set BOOT0 high via a jumper and boot into the bootloader.  The Linux  'dmesg' command shows: [3552008.377434] usb 3-2: new full-speed USB device num...

LMorr.3 by Senior II
  • 2047 Views
  • 2 replies
  • 0 kudos

Resolved! DfuSe does not read the device

Hi there,I applied the DfuSe Demo to connect it to the NanoVna and make somemeasurements.But, when I connected the NanoVna I had no luck; I mean the DfuSe does not read the device.

MAlsu.1 by Associate
  • 5748 Views
  • 5 replies
  • 4 kudos

STM32CubeProgrammer download link not working.

Every time I try and download any version for any OS it just takes me to the License Agreement and when I except just loops me back to the "Get Software" page with no download beginning. I tried 3 browsers and 2 different laptops. Any other download ...

Pigeon by Associate II
  • 3349 Views
  • 8 replies
  • 0 kudos

Wrong elf file download.

Hello, I use cube programmer. The chip I use is STM32H743ZGT6, but I accidentally downloaded the elf file of STM32H735VGT6.So I tried to download it again, but the st-link itself won't connect. How can I fix this?

giwonKIM by Associate III
  • 2451 Views
  • 5 replies
  • 2 kudos

Problems installing SFI on STM32U575

Hello,I am trying to install a SFI file on a STM32U575 microcontroller. I have generated the SFI with a binary (0x08000000) and at the time of installing the SFI, I get the following error:Error: Execution of RSS CMD failed, returned value = 0x1 Erro...

problema sfi.png
mikel-m by Associate III
  • 1118 Views
  • 1 replies
  • 0 kudos

Installation Issues - Infinite Loop

I've got a brand new VM running Windows 11 pretty much off the shelf. I can install and run Cube IDE but when I try to install the STM32CubeProgrammer (64 bit version) I get into an infinite loop where the following happens:- It opens the Install Wiz...

thayden by Associate II
  • 7446 Views
  • 12 replies
  • 5 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.