STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

SetupSTM32CubeProgrammer-2.17.0.exe failed

I got this error message when trying to install the cube programmer:This application was configured to use a bundled java runtime environment but the runtime is missing or corrruptedI have started an jar file to see if my local jre is broken which is...

HeinzH_0-1720015336386.png HeinzH_1-1720015437731.png
HeinzH by Associate
  • 3227 Views
  • 4 replies
  • 0 kudos

stm32WB. How to reset to factory settings?

Hello,  I have a problem with the return of the STM32WB to the factory settings  When I use the next command  STM32_Programmer_CLI.exe -c port=SWD -w32 0x5800040C 0x00008000 that looks like that  But finally, when I read FUSE I saw that Stake was no...

08bf8040-d86f-4e8c-8268-a610e0253820 (1).jpeg FUS.jpg
Ronil by Senior
  • 1913 Views
  • 1 replies
  • 0 kudos

Resolved! Updating STM32F373 over USB DFU Fails to Connect

I'm able to connect to my STM32F373 board over a USB virtual port com successfully.  I'm also able to set BOOT0 high via a jumper and boot into the bootloader.  The Linux  'dmesg' command shows: [3552008.377434] usb 3-2: new full-speed USB device num...

LMorr.3 by Senior II
  • 1960 Views
  • 2 replies
  • 0 kudos

Resolved! DfuSe does not read the device

Hi there,I applied the DfuSe Demo to connect it to the NanoVna and make somemeasurements.But, when I connected the NanoVna I had no luck; I mean the DfuSe does not read the device.

MAlsu.1 by Associate
  • 5556 Views
  • 5 replies
  • 4 kudos