STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Flash Loader in Nucleo-STM32F401 (Unrecognized device)

Hi everyone.I have a board Nucleo-STM32F401, and i will try to write the program on STM32f401 with RS-232 communication, i did like in pdf, BOOT0 with jumper connect to Vcc (CN7 5pin+7pin) and i have the simple device RS232 to USB, and RX/TX connect ...

OMarc.1 by Associate III
  • 1328 Views
  • 2 replies
  • 0 kudos

Program STM32 through bus CAN

Hello,Is it possible to program STM32* through bus CAN with STM32CubeProgrammer and STLINK-V3SET ?If yes :can we program only one STM32* even if many other STM32* are connected to the bus ?do we need to flash a bootloader or the embedded bootloader i...

ValentinG by Associate II
  • 1221 Views
  • 2 replies
  • 0 kudos

How to disable TZEN?

I try to unselect the TZEN flag to set it to 0 using STM32CubeProgrammer and it keeps reading back 1 after clicking apply.

Konami by Senior II
  • 1448 Views
  • 2 replies
  • 0 kudos

DFU not working on any STM32 board

NUCLEO boards are all not doing DFU: G031K8, L031K6, G431KB, G431RB, L452RE, L476RG, F401RE and of course the H743ZI the first version with STLINK2 None of those boards are seen by STMCUBE Programmer, in Windows 10 Device Manager USB section I never ...

KevinA by Senior
  • 1166 Views
  • 3 replies
  • 0 kudos