Skip to main content
Konami
Senior
September 11, 2019
Question

How to disable TZEN?

  • September 11, 2019
  • 2 replies
  • 1000 views

I try to unselect the TZEN flag to set it to 0 using STM32CubeProgrammer and it keeps reading back 1 after clicking apply.

This topic has been closed for replies.

2 replies

Jocelyn RICARD
ST Employee
October 23, 2019

Hello Konami,

the STM32L5 is not available yet for mass market so the support on this chip is should go through your FAE.

Such information will be available with documentation and training that will be provided at same time as mass market launch.

By the way, setting TZEN back to 0 requires making a regression from RDP1 to RDP0. This information is available in the RM

But be careful, when in RDP1 you can only attach to the target in non secure mode. So, you must have a SW running on the target that starts in secure and switches in non secure. Then you can attach in hotplug and do the regression; TZ=0 RDP=0xAA

Best regards

Jocelyn

Martin.Sergio
Associate III
January 27, 2020

Hello Konami,

I have the same problem, Have you fixed it?

Best Regards

Sergio