STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Option Bytes break Cube Programmer connection

I am trying to flash a STM32F303CCT6, and any time I try to set the Option Bytes to Level 1 protection it locks the board and breaks the connection. The only thing that is able to both see, and wipe the board is an android app.The board has WinUSB on...

STM32CubeProgrammer - No ST-LINK Detected

Hi all, I have been struggling to get Atollic 9.3.0 to start a debug session, failing at the load point where it tries to use the STM32CubeProgrammer CLI (1.3.0 in that release of Atollic).I thought I would download the STM32 ST-LINK Utility and this...

MWill.18 by Associate II
  • 7102 Views
  • 8 replies
  • 0 kudos

STM32CubeProgrammer 2.2.0 released

Dear communityWe are pleased to announce the release of STM32CubeProgrammer 2.2.0New features • Added the support of the STM32L5 Series • Added the support of HSMv2 • Added the support of IAP for the USB-DFU interface • STM32WB firmware upgrade via t...