cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F401 NUCLEO-64 RS-232 Bootloader Flash Loader Demonstration/STM32CubeProgrammer

OMarc.1
Associate III

Hi, Everyone.

I have a board STM32F401 NUCLEO-64 and i try to use bootloader with RS-232.

I am using PA10 and PA9 like RX/TX. 

On CN7 i connect pins 5 and 7 (BOOT0 to 3,3V).

On CN10 pins 20 and 22 (BOOT1 to GND).

For RS-232 i am using cables USB to RS-232, and i try to connect without cable USB-R232, solder D-SUB 9 pin, (pins 2,3 and 5) and connect on COM-port on PC.

And I always have a message on Flash Loader Demonstration

Unrecognized device.

I tried to click the reset pin, and other things.

in STM32CubeProgrammer i have next message

Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again...

I saw and did like in video instruction, and i always have problems.

Power supplies i used different, and from USB, and used the separate power supply (of course with connected to GND).

On the oscilloscope, i see impulses RX and TX, when i try to connect. 

Kind regards,

Oleksii

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0