STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Can't close app, if connection was failed.

Hello, i found next problem. If open app, and try connect to board with unsuccessful result, than app can't be closed any method, other than via task manager. In other case, app close via stantard button. This bug not disapering, if, for example, fir...

PGorb.1 by Associate
  • 3929 Views
  • 15 replies
  • 0 kudos

Resolved! How do I setup my Embitz to Debug with new L4Q5 MCUs ?

Hi everyone,I migrated to L4Q5 MCU and the Embitz debugger is not able to see the Target. I have pointed the build options to the new linker file. However, I feel like I need to translate STM32CubeProgrammer settings to the Embitz debugger options. W...

0693W000005AEn7QAG.png
VNado.1 by Associate III
  • 3032 Views
  • 6 replies
  • 0 kudos

Can't build API examples. Library issues! Help!

:-1: error: /home/serg/STMicroelectronics/STM32Cube/STM32CubeProgrammer/api/project/Qt/STM32CubePrgAPI/../../../../lib//./libQt5Xml.so.5: undefined reference to `QXmlUtils::isPublicID(QString const&)@Qt_5_PRIVATE_API'Qt Creator 4.7.1Based on Qt 5.11....

SSolo.2 by Associate II
  • 1444 Views
  • 0 replies
  • 0 kudos

stm32l515cb no debug with gdb only openocd

We can not user gdb for debug with our board. We can not user stm32programmer eitherIt works correctly with stlink and debug with openocd.the strange thing is that stm32cube programmer connects correctly to the device but recognizes it as stm32l0.wha...

0693W0000059tJbQAI.png 0693W0000059tJpQAI.png
PVale.2 by Associate
  • 593 Views
  • 0 replies
  • 0 kudos