cancel
Showing results for 
Search instead for 
Did you mean: 

Bug: STM32CubeProg 2.3.0 doesn't recognize S-record files.

Andrei Chichak
Lead II

In the Erasing & Programming tab the file path browse button dialog will not allow me to select an s-record file, even if the file type is s19, srec, or Srec.

Thanks.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Hi @Andrei Chichak​ 

Please try with the last STM32CubeProgrammer version then tell me if it solve the issue.

Best regards,

Nesrine

Andrei Chichak
Lead II

Yes, I see that 2.5.0 now understands .srec files.

ST's previous ventures DeFUse/DFU File Manager, and the Flash Loader Demonstrator chose to recognize the .s19 suffix instead of .srec. Is there any chance that your wizards could add .s19 as an alternative to .srec? Like recognize both?

Thanks,

Andrei