STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Flash NUCLEO-H743 with UART in CubeProgrammer

I have NUCLEO-H743 board. After I load the firmware with this pin configuration, the board began to give an error STLINK (PB4 is NJTRST). Initially, the board was flashed even with this configuration, but after Debugging it stopped. I was advised to ...

0693W000008yaFTQAY.png 0693W000008yaFOQAY.png
MZoto.1 by Associate
  • 1155 Views
  • 1 replies
  • 0 kudos

Via following the Keil official document(Programming External Flash used with STM32 Devices MDK Tutorial ), I write a Keil MDK external flash for the custom STM32F767 board. Erase Chip and Program are done but verify encounters errors (Contents mismatch a

As title. In order to test the external loader algorithm, I add a test data to a QSPI project that can be excuted correctly when downloaded to the internal flash. The test data will be written in the external flash via the external download algorith...

0693W000008yjLQQAY.png 0693W000008yjLkQAI.png 0693W000008yjLzQAI.png 0693W000008yjMOQAY.png
KaoChin by Associate
  • 1445 Views
  • 0 replies
  • 0 kudos

stm32 Cube Programmer Window does not close

I have downloaded the latest version of Cube Programmer and updated my ST-LINK/V2 firmware. I've tried to program connect with a target I have designed and the target cannot be found. Clearly I need to find out why, but that is not my question. Rath...